Tower Lights and Beacons XVB—70 mm Diameter (2.75 inches) XVC, 40 mm, 60 mm, and 100 mm Diameter Signaling Units XVR Pre-Wired Rotating Mirror Beacons XVS Sirens and Electronic Alarms Parent topic: Push Buttons and Operator Interface