Solution Center Workflows
The Solution Center subtab, or workflow family, is the home of client-side workflows specific to the Solution Center application. Currently, that consists of the Recomplete Edit Assignment workflow.
This is a client-side workflow that is meant to complete an edit assignment on a session which stopped progressing to its next assignment due to an error. A user may create a session and complete work on the session, send for approval, but the session does not show up in the approval assignment or review assignment. This powerful tool allows this session to be recovered by completing its edit assignment so that the session is then visible to the right users, and made available for review or approval.
Below is an example of a Solution Center workflow, the Recomplete Edit Assignment workflow.
Once an administrator learns of a session that stopped progressing, they can go to Run History to learn how to execute the Recomplete Edit Session workflow.
Available Tools
The functions, tools, and subtabs are largely the same between the Studio and Default Workflow Studio tabs. However, the Studio tab provides a few additional tools on its subtabs. Refer to the Studio topic to learn about the additional tools.
The following buttons are available on all subtabs in Default Workflow Studio:
Revision history of a workflow is recorded and can be helpful to track changes made to different versions of workflows over time. Refer to the Default Workflow Studio topic to read more about revision history records.
Workflow Properties
| Property | Definition |
|---|---|
|
Name |
The title of your workflow. |
|
Minimum Client Version |
The minimum version of Editor required to execute this workflow. This field applies to autoupdater workflows on the ArcGIS Server subtab, and workflows on the Editor Client subtab. Drop-down values on the ArcGIS Server subtab begin with 2024 C1. Drop-down values on the Editor Client subtab begin with 2025 C1. We recommend leaving this field blank on all other types of workflows. |
|
Workflow Status |
Published — the workflow is published and represents the latest version of the workflow. Draft — the workflow is in draft form and not published. Retired — the workflow has been replaced by a newer version and this version is retired and no longer published. Example — this is a workflow example that is useful for copying and pasting into a new workflow as a template or starting point. |
|
Workflow Metadata Id |
The unique identifier on each version of a workflow that allows you to call a particular version. |
|
Workflow Ancestral Id |
This identifier designates the starting point of a workflow’s history, after which all versions maintain that Ancestral Id. |
|
Version |
The version number of the workflow. Useful in tracking the evolution of workflows as administrators make changes. |
|
Updated By |
The user name of the last person to modify the workflow. The OOTB workflows provided by Schneider Electric say Updated By Schneider Electric Team, or sometimes say none. |
|
Updated On |
The date the last workflow modifications were made. |
|
Expression Language |
The coding language that is used within the workflow. |