Workflow Filters

On the Run History tab, at the top of the list of workflows are two filters.

  • View Only Workflows with Errors: This reduces the list to only dynamic workflows that have encountered an error.

  • Filter Workflows by Type: This allows you to filter the list by workflow. You can pick one or more workflows (the images below represent examples so you likely have more choices).

    Example for Mobile XI:


    Example for Designer XI, Editor XI, DHFC, Feeder Services, and GDBM:


QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?