Workflow Search

The Search field at the top of the interface allows you to search by Design ID, Session ID, or Markup ID, to filter the list of workflow entries. The Search field uses Cosmos DB language, so the best way to search is to let the application provide the syntax for you. To do so, follow these steps:

  1. In the app you’re using, locate the design, session, or markup that passed through (or is currently passing through) a dynamic workflow.

  2. Click the design, session, or markup to highlight it in green. Then, click the View Workflow History button. The following are a few examples from various XI series applications:

    • ArcFM Mobile:

    • Designer XI:

    • Editor XI:

  3. The View Workflow History button toggles you back to the Workflows plugin > Run History tab, and it populates the Search field with the appropriate ID.

You are now ready to explore the dynamic workflow further.


QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?