Test Cases
Test Cases can be used to test a workflow without connecting to any services. If you started with a workflow from the Default Workflow Studio, it came with a variety of pre-written scenarios.
On the Test Cases subtab, you run your workflow through a variety of scenarios to ensure it can complete its tasks, given specified arguments and criteria.
Click on a test case to highlight it in green. This populates the middle pane of the interface.
There are four subtabs: Basics, Responses, Events, and Output Assertion,
plus a Draw Desired Path button and a Run Test
button.
-
Draw Desired Path: This highlights the paths covered by the current test case.
-
Run Test: This initiates the current test case.
-
Basics: This provides high-level information about the test case, including Title, Initial State, and Nodes Visited.
-
Responses: This allows you to simulate the expected results from a web service call.
-
Events: This allows you to simulate expected service bus messages.
-
Output Assertion: After the test case is complete, this confirms an expected value in an object.