Graph

On the Graph subtab you can design, modify, and run workflows. Building a workflow is performed by arranging stages of a workflow:

  • The graph is for visualization of a workflow.

  • C# code or Javascript can be used in key places to customize the code.

  • You can download workflow information and edit in a text editor.

  • All design work happens on the left-hand side of the interface, and the graph on the right-hand side adjusts as you work.

  • The Graph subtab uses syntax from the open source graph visualization software GraphViz.

    NOTE: Exceptions to the GraphViz syntax are all arguments that have the prefix “se_”. These are specific to Schneider Electric functionality.


Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.