GEX8258701EN-01

Performance of Outdoor Side-Mounted Cooling Units

  • Ti: Internal temperature of the enclosure

  • Ta: Ambient temperature

  • P: Cooling capacity

Commercial reference

Cooling capacity

L35-L35

Cooling capacity

L35-L50

Performance

W (BTU/h)

W (BTU/h)

NSYCUHD350DG

340 (1160.1)

220 (750.7)

NSYCUHD600DG

630 (2149.6)

460 (1569.6)

NSYCUHD800DG

800 (2729.7)

540 (1842.6)

NSYCUHD1KDG

NSYCUHD1K2P4DG

990 (3378)

710 (2422.6)

NSYCUHD1K6DG

NSYCUHD1K62P4DG

1630 (5561.8)

1350 (4606.4)

NSYCUHD2K3P4DG

1990 (6790.2)

1550 (5288.9)

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?