GEX8258701EN-01

Installation of Indoor Side-Mounted Cooling Units

Dimensions and Cutouts

The overall dimensions, position of the fixing points and cutout of the indoor side-mounted cooling units can be downloaded from our website at www.se.com/ww/en/download.

The table below gives links to open the dimensions file for each commercial reference:

Commercial reference

Dimension file name

NSYCU350DG

NSYCUX350DG

NSYCU600DG

NSYCUX600DG

GEX8130602

NSYCU800DG

NSYCU8002P4DG

NSYCU1KDG

NSYCUX1KDG

GEX8136102

NSYCU1K2P4DG

NSYCUX1K2P4DG

NSYCU1K2DG

NSYCU1K22P4DG

NSYCU1K6DG

NSYCUX1K6DG

NSYCU1K62P4DG

NSYCU2KDG

NSYCU2K3P4DG

NSYCUX2K3P4DG

GEX8215402

NSYCU3K2DG

NSYCU3K23P4DG

NSYCU4K3P4DG

GEX8218002

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?