GEX8258701EN-01

External Water Condensate Evaporator

DANGER
hazard of electric shock
Only specialized personnel are allowed to maintain and clean the external evaporator. The personnel must ensure that for the duration of the maintenance and cleaning, the external evaporator is disconnected from the electrical supply.
Failure to follow these instructions will result in death or serious injury.
CAUTION
hazard of burning from hot surfaces
  • Do not touch external and internal surfaces during operation.
  • Let the external surfaces cool after the cooling unit has been switched off.
  • Do not try to touch water tray during operation
Failure to follow these instructions can result in injury or equipment damage.

Presentation

The external condensate water evaporator is compatible with indoor side and roof-mounted cooling units. It helps to ensure that the condensate water is actively evaporated with an electrical resistance.

The external evaporator is particularly recommended for cooling units with a cooling capacity less than 800 W as they are not equipped with a passive evaporator.

Technical Data

Characteristics

Value

Height x width x depth

103 x 164 x 148 mm (4.1 x 6.5 x 5.8 in)

Implementation

External mounting

Weight

1.2 kg (2.6 lb)

Material

Powder-coated mild steel

Color

RAL 7035

Electrical data

Voltage

230 Vac

Frequency

50/60 Hz

Starting current

2 A

Power consumption
  • During operation (max. heater fully immersed)

  • Standby (dry)

  • 230 W

  • 25 W

Performance

Evaporation rate

0.25 l/h

Dimensions

Installation Instructions

Install the external evaporator at a minimum distance of 60 mm (2.36 in) below the cooling unit.

Condensate will form on the bottom of the cooling unit. To minimize the amount of condensate, maximize the distance between the cooling unit and the evaporator, and provide adequate ventilation.

Installation Procedure

  1. Drill the necessary holes in the side of the enclosure, below the cooling unit.

  2. Position the external evaporator on the side of the enclosure, aligning holes.

  3. Insert and tighten the screws provided.

  4. Connect the hose to the water condensate drain connection of the cooling unit.

  5. Insert the hose into the hole in the top of the external evaporator.

  6. Connect the power supply for the external evaporator.

Wiring Diagram

 
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.