GEX8258701EN-01

Enclosure Transportation With Cooling Unit Mounted

NOTICE
temperature, humidity, dropping, and impact damage
  • Do not expose the cooling unit to temperatures above 70 °C (158 °F) or below -20 °C (-4 °F), and/or relative humidity above 95%.
  • Use adequate packing for shipping, and avoid shocks and impacts.
Failure to follow these instructions can result in equipment damage.
  • To transport the enclosure with the cooling unit installed, place it on a pallet with dimensions greater than the assembly. Protect the cooling unit with its own container during transport.

  • Always transport the enclosure in a vertical position.

  • Before connecting the cooling unit, wait 30 minutes for the lubricant oil to accumulate in the compressor.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?