GEX8258701EN-01

Surface Mounting Installation Procedure

Follow this procedure to install a surface-mounted cooling unit.

  1. Open the enclosure door.

  2. Make the necessary cutouts in the door or side panel of the enclosure.

  3. Use a crane to position the cooling unit against the cutouts, with the bar bracket above the bottom edge of the top cutout.

  4. Slide the cooling unit down to fix it in position.

  5. Use a size 10 hexagonal key and the bolts and washers provided to fix the cooling unit in place. Tighten to a torque of 4.5 N•m (40 lb-in).

  6. Remove the lifting ring.

  7. Connect the water condensate removal hose provided (1 m (3.28 ft)) to the drain connection.

    NOTE: An external water condensate evaporator can be connected to the drain connection.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?