Disposal and Recycling
| NOTICE |
|---|
|
hazard of environmental harm
Failure to follow these instructions can result in equipment damage.
|
When the life cycle of the cooling unit comes to an end, proceed as follows:
-
Drain the refrigerant contained in the cooling system.
-
Drain the lubricant oil contained in the compressor.
-
Draining fluids and oils should be carried out by trained personnel with the necessary means to collect oils and gases so they do not spill into the external environment.
-
Disassemble and subdivide the internal elements to carry out a diverse collection for the recovery of materials (steel, copper, aluminum, plastic, etc.).
During disassembly, keep the cooling unit:
-
Vertical for side-mounted cooling units
-
Horizontal for roof-mounted cooling units
In all cases, take into account the existing regulations in the country where it is being used.