GEX8258701EN-01

Use Procedures

NOTICE
damage from unauthorized programming
Schneider Electric will not be held responsible if the user modifies the programmed parameters without due authorization.
Failure to follow these instructions can result in equipment damage.

Setting the Temperature Setpoint

  1. Press and release SET to access the ClimaSys cooling unit status menu.

  2. Scroll through the folders using the keys and until you find the folder SEt

  3. Press SET to view the current setpoint value.

    NOTE: The default value of the setpoint is 35 °C (95 °F)
  4. Change the setpoint value using the keys and within 15 seconds.

  5. To confirm the value press SET or , or wait for the 15 seconds timeout.

NOTE:
  • The compressor has a minimum ON time of 3 minutes. If the temperature setpoint is set below the enclosure temperature and the compressor has been ON for less than 3 minutes, then the compressor will continue running until the minimum ON time is respected.

  • The compressor has a minimum OFF time of 4 minutes. If the temperature setpoint is set above the enclosure temperature and the compressor has been OFF for less than 4 minutes, then the compressor will start only after the minimum OFF time has elapsed.

ClimaSys Cooling Unit Status Menu

To enter the ClimaSys cooling unit status menu:

  1. Press and release SET.

  2. Scroll through the folders using the keys and and until you find the label for the desired folder.

  3. Press and release SET.

  4. View the value reading.

  5. To exit press SET or , or wait for the 15 seconds timeout.

The folders shown are as follows:

SEt: Setpoint setting folder

ALr: Alarms folder (only visible if there are active alarms )

rtC: Clock parameters folder

  • dAy: Day

  • h: Hour

  • ‘ : Minutes

Pb1: Pb1 probe value folder

idF: Firmware mask value folder

rEL: Firmware release value folder

nAM: Product name folder

Programming Menu

To enter the Programming menu and access the user parameters:

  1. Press and hold SET for at least 5 seconds .

  2. Scroll to PA1. Press SET to enter PA1 password using the keys and . Press SET to confirm.

  3. Upon access the first parameter (HAL) will be shown.

  4. Scroll through the parameters using the keys and until you find the label for the parameter you want to change.

  5. Press and release SET.

  6. Set the desired value using the keys and .

  7. To confirm the value press SET or , or wait for the 15 seconds timeout.

NOTE: Switch the device off and on again every time you change the parameter configuration.

Viewing Measured Temperature Value

  1. Press and release SET to access the ClimaSys cooling unit status menu.

  2. Scroll through the folders using the keys and until you find the folder Pb1.

  3. Press SET to view the value measured by the corresponding probe.

NOTE: The displayed value cannot be changed.

Passwords

PA1 password: 5

PA2 password: Not available for user. Please contact the Customer Care team.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?