GEX8258701EN-01

Stand-alone Mode

Description

Follow this procedure to return back to normal mode (stand-alone). Check that the cooling unit is On before returning to normal mode.

Setting Procedure

Enter the Programming menu:

  1. Press and hold SET for at least 5 seconds.

  2. Scroll to PA1. Press SET to enter PA1 password using the keys and Press SET to confirm.

Set the cooling units:

  1. Scroll to H13 and press SET.

  2. Change value to -4 using the keys and . Press SET to confirm.

  3. Scroll to H11 and press SET.

  4. Change value to 0 using the keys and . Press SET to confirm.

The changes made to the parameters are taken into account after powering Off and On the cooling units.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?