GEX8258701EN-01

Filter Replacement

The table below describes which filter to use according to the cooling unit environment.

Cooling unit environment Filter recommendation

Office (no dust, no grease)

No filter required

Industrial (dust, grease, non-explosive atmosphere)

Filter required

Outdoor

Aluminum filter required

No filter is delivered with indoor cooling units.

An aluminum filter is delivered with outdoor cooling units.

For more information about filters, refer to Accessories.

Installing a Filter in an Indoor Cooling Unit

No filter is delivered with the indoor cooling unit. To install or replace a filter in an indoor cooling unit, follow this procedure:

  1. Slide the filter through the cutout in the lateral side of the cooling unit.

Replacing Filter in an Outdoor Cooling Unit

Outdoor cooling units are delivered with an aluminum filter fitted. To replace an aluminum filter in an outdoor cooling unit follow this procedure:

  1. Locate the slot cover at the bottom of the cooling unit and unscrew the 2 screws with a T10 Torx screwdriver.

  2. Remove the slot cover.

  3. Slide out the used filter.

  4. Insert the new filter in the slot.

  5. Reposition the slot cover.

  6. Screw the 2 screws back into place with a T10 Torx screwdriver.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?