GEX8258701EN-01

Alarms and Indications

All alarms are deactivated automatically when their cause is removed.

Detecting an Alarm Condition

If there is an alarm condition, the alarm icon comes on steadily and the alarm code is displayed. If present and enabled, the alarm relay is also activated.

NOTE: If alarm exclusion timings are in progress, the alarm is not signaled.

All active alarms, except those relating to probe error, are listed in the ALr folder within the ClimaSys cooling unit status menu.

Silencing an Alarm

Press any key or use the menu function: the alarm icon flashes, and the alarm relay is de-energized.

The alarm icon goes off when the alarm condition disappears.

Alarms Legend


Code

Description

Alarm relay

Cause

Effects

Solutions

E1

Probe Pb1 error

Active

  • Reading of values outside the operating interval.

  • Probe or corresponding wiring in short-circuit or open circuit.

  • E1 code displayed

  • Steady alarm icon

  • Compressor operation based on parameters Ont and OFt.

  • Check the probe wiring.

  • Replace the probe.

AH1

Alarm due to Pb1 HIGH temperature

Active

Value read by probe Pb1 > HAL

  • Alarm AH1 added to folder ALr.

  • No effect on regulation.

Wait for the temperature read by Pb1 to drop below the alarm threshold (HALAFd).

AL1

Alarm due to Pb1 LOW temperature

Active

Value read by probe Pb1 < LAL

  • Alarm AL1 added to folder ALr.

  • No effect on regulation.

Wait for the temperature read by Pb1 to rise above the alarm threshold (LAL +AFd).

oPd

Open door alarm

Active

Digital input activation (H1x = ±4) .

  • Alarm oPd added to folder ALr.

  • Steady alarm icon .

Close the door.

Wrong phase order for three-phase cooling units alarm

Active

Wrong phase order during commissioning.

  • Alarm oPd added to folder ALr.

  • Steady alarm icon .

Connect power cables following power supply connection.

Setting the High Temperature Alarm (HAL)

  1. Press SET and hold for at least 5 seconds. Scroll to PA1. Press SET to enter PA1 password using the keys and . Press SET to confirm.

  2. Scroll using the keys and to HAL and press SET. Default value 50.

  3. Change value using the keys and . Press SET to confirm or to cancel.

Setting the Low Temperature Alarm (LAL)

  1. Press SET and hold for at least 5 seconds. Scroll to PA1. Press SET to enter PA1 password using the keys and . Press SET to confirm.

  2. Scroll using the keys and to LAL and press SET. Default value 0.

  3. Change value using the keys and . Press SET to confirm or to cancel.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?