GEX8258701EN-01

Modbus Daisy Chain

NOTICE
unintended equipment operation
  • Disconnect all the equipment before installing/dismantling cables or wires.
  • Seal the connections in compliance with the technical specifications relating to the tightening torque.
  • Correctly position and adequately secure the converter inside the equipment to avoid disconnection.
  • The load equivalent to the entire RS-485 bus should not exceed 8 Unit Load (Refer to standard TIA/EIA-485–A for the definition of a Unit Load.)
  • Do not fit the termination resistors inside the RS-485 network.
  • For the connection with the supervision system, use specific data-cable such as BELDEN cable model 8762 that are shielded and twisted.
  • The RS-485 communication cables must be routed separately from the power cables.
Failure to follow these instructions can result in equipment damage.

GND: Ground

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?