GEX8258701EN-01

Internal Wiring Diagrams

This section shows the internal wiring diagrams according to the supply voltage and the commercial reference of the cooling unit.

Legend of the symbols used in the internal wiring diagrams:

Si: Internal temperature sensor

Hcc: Compressor with case heater (for outdoor cooling units)

Cc: Compressor capacitor

Ps: DC power supply

Ci: Internal fan capacitor

Ca: Ambient fan capacitor

Mc: Compressor

Ma: Ambient fans

Mi: Internal fan

CC: Contactor

Supply voltage

Commercial reference

Diagram

1 x 230 Vac +N

NSYCU350DG

NSYCUX350DG

NSYCU600DG

NSYCUX600DG

NSYCUHD350DG

NSYCUHD600DG

NSYCU600RDG

1 x 230 Vac +N

NSYCU800DG

NSYCU1KDG

NSYCUX1KDG

NSYCU1K2DG

NSYCU1K6DG

NSYCU1K6DG

NSYCU2KDG

NSYCU3K2DG

NSYCUHD800DG

NSYCUHD1KDG

NSYCUHD1K6DG

NSYCU800RDG

NSYCU1K2RDG

NSYCU1K5RDG

NSYCU2KRDG

(1) Used only for roof-mounted cooling units above 1.2 kW and 3 kW side-mounted cooling units.

2 x 400/460 Vac

NSYCU8002P4DG

NSYCU1K2P4DG

NSYCUX1K2P4DG

NSYCUHD1K2P4DG

NSYCU1K22P4DG

NSYCU1K62P4DG

NSYCUHD1K62P4DG

(1) Used only for roof-mounted cooling units above 1.2 kW.

3 x 400/460 Vac

NSYCU2K3P4DG

NSYCUX2K3P4DG

NSYCUHD2K3P4DG

NSYCU2K3P4RDG

NSYCU3K23P4DG

NSYCU3K3P4RDG

NSYCU4K3P4DG

NSYCU4K3P4RDG

(1) Used only for 3 kW and 4 kW cooling units.

(2) Used only for 2 kW roof-mounted cooling units.

(3) Used only for 2 kW wall-mounted cooling units without pressure switch.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?