GEX8258701EN-01

Half-Flush Mounting Installation Procedure

Half-Flush Mounting Kit

Use the half-flush mounting kit suitable for your cooling unit to install the cooling unit. Check the table below for compatibility.

Cooling unit commercial reference

Half-flush mounting kit

NSYCU350DG

NSYCU600DG

NSYCUACC034DG

NSYCUX350DG

NSYCUX600DG

NSYCUACC038DG

NSYCU800DG

NSYCU8002P4DG

NSYCU1KDG

NSYCUACC035DG

NSYCUX1KDG

NSYCUACC039DG

NSYCU1K2P4DG

NSYCU1K2DG

NSYCU1K22P4DG

NSYCU1K6DG

NSYCU1K62P4DG

NSYCU2KDG

NSYCU2K3P4DG

NSYCUACC036DG

NSYCUX1K2P4DG

NSYCUX1K6DG

NSYCUX2K3P4DG

NSYCUACC040DG

NSYCU3K2DG

NSYCU3K23P4DG

NSYCU4K3P4DG

NSYCUACC037DG

Installation Procedure

Follow this procedure to install the cooling unit with a half-flush mounting.

  1. Open the enclosure door.

  2. Make the necessary cutout in the door or side panel of the enclosure.

    NOTE: To install the cooling unit in the side panel using a half-flush mounting, the side panel must be taken off.
  3. Install sealing tape around the front face of the mounting kit. Check that the ends of the tape meet without leaving a gap.

    NOTICE
    hazard of loss of ip55 protection
    When installing the cooling unit, check that the ends of the sealing tape meet without leaving a gap.
    Failure to follow these instructions can result in equipment damage.

  4. Position the mounting kit on the back of the door or side panel against the cutout.

  5. Screw into place using size 10 hexagonal key and the bolts and washers provided. Tighten to a torque of 4.5 N•m (40 lb-in).

  6. Use a crane to position the cooling unit in the mount.

  7. Use a size 10 hexagonal key and the bolts and washers provided to fix the cooling unit in place. Tighten to a torque of 4.5 N•m (40 lb-in).

  8. Remove the lifting ring.

  9. Connect the water condensate removal hose provided (1 m (3.28 ft)) to the drain connection.

    NOTE: An external water condensate evaporator can be connected to the drain connection.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?