GEX8258701EN-01

Performance of Indoor Roof-Mounted Cooling Units

  • Ti: Internal temperature of the enclosure

  • Ta: Ambient temperature

  • P: Cooling capacity

Commercial reference

Cooling capacity

L35-L35

Cooling capacity

L35-L50

Performance

W (BTU/h)

W (BTU/h)

NSYCU600RDG

620 (2115.5)

470 (1603.7)

NSYCU800RDG

NSYCU8002P4RDG

810 (2763.8)

550 (1876.6)

NSYCU1K2RDG

NSYCU1K22P4RDG

1280 (4367.5)

810 (2763.8)

NSYCU1K5RDG

NSYCU1K52P4RDG

1480 (5049.9)

1140 (3889.9)

NSYCU2KRDG

1960 (6687.7)

1630 (5561.7)

NSYCU2K3P4RDG

2090 (7131.4)

1580 (5391.2)

NSYCU3K3P4RDG

3170 (10816.4)

2470 (8427.9)

NSYCU4K3P4RDG

3890 (13273.2)

3170 (10816.4)

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?