Sequential Mode
Description
The SY1 SY2 contacts of the synchronization mode terminal of two cooling units with the same commercial reference are connected in parallel.
At start-up, regulation is managed by cooling unit 1. Cooling unit 2 is in standby.
When cooling unit 1 reaches the t01 compressor working hours (h*10), it closes the synchronization output and goes into standby. Cooling unit 2 reads the synchronization signal and becomes operative for t01 compressor working hours. When cooling unit 2 reaches t01 compressor working hours, it goes into standby and cooling unit 1 starts again.
In case of High Temperature Alarm HAL for any of the cooling units, the alarm starts without waiting for the sequential time.
Setting Procedure
Enter the Programming menu:
-
Press and hold SET for at least 5 seconds.
-
Scroll to PA1. Press SET to enter PA1 password using the keys
and
. Press SET to confirm.
Set cooling unit 1:
-
Scroll to H11 and press SET.
-
Change value to +15 using the keys
and
Press SET to confirm.
-
Scroll to t01 and press SET.
-
Change value for working hours (h*10) using the keys
and
. Press SET to confirm. The default value is 1 (10 hours).
Set cooling unit 2:
-
Scroll to H11 and press SET
-
Change value to -15 using the keys
and
. Press SET to confirm.
-
Scroll to t01 and press SET.
-
Change value for working hours (h*10) using the keys
and
. Press SET to confirm. The default value is 1 (10 hours).
The changes made to the parameters are taken into account after powering Off and On the cooling units.