Installation of Outdoor Side-Mounted Cooling Units
Dimensions and Cutouts
The overall dimensions, position of the fixing points and cutouts of the outdoor side-mounted cooling units can be downloaded from our website at www.se.com/ww/en/download.
The table below gives links to open the dimensions file for each commercial reference:
|
Commercial reference |
Dimension file name |
|---|---|
|
NSYCUHD350DG NSYCUHD600DG |
|
|
NSYCUHD800DG NSYCUHD1KDG NSYCUHD1K2P4DG |
|
|
NSYCUHD1K6DG NSYCUHD1K62P4DG NSYCUHD2K3P4DG |
Outdoor Mounting Installation Procedure
Outdoor side-mounted cooling units must be surface mounted in the same way as for indoor surface-mounted units. Half-flush and flush mounting are not suitable for outdoor side-mounted cooling units.