GEX8258701EN-01

Flush Mounting Installation Procedure

Follow this procedure to install the cooling unit with a flush mounting.

  1. Loosen the four screws of the cooling unit cover by turning them anticlockwise through 90° using a PZ2 screwdriver. The screws remain in their housing.

  2. Remove the cover of the cooling unit.

  3. Install sealing tape around the flange. Check that the ends of the tape meet without leaving a gap.

    NOTICE
    hazard of loss of ip55 protection
    When installing the cooling unit, check that the ends of the sealing tape meet without leaving a gap.
    Failure to follow these instructions can result in equipment damage.

  4. Open the enclosure door.

  5. Make the necessary cutout in the door or side panel of the enclosure.

    NOTE: To install the cooling unit in the side panel using a flush mounting, the side panel must be taken off.
  6. Use a crane to position the cooling unit on the back of the door or side panel with the flange protruding through the cutout.

  7. Screw into place using size 10 hexagonal key and the bolts and washers provided. Tighten to a torque of 4.5 N•m (40 lb-in).

  8. Loosen the 4 screws holding the thermostat mounting by turning them anti-clockwise through 90°.

  9. Slide forward the thermostat mounting to the maximum. The final position allows the thermostat and the protection plate to align.

  10. Tighten the 4 screws by turning them clockwise through 90°.

  11. Place the cooling unit cover on to the front of the cooling unit.

  12. Tighten the four screws clockwise through 90° using a PZ2 screwdriver.

  13. Remove the lifting ring.

  14. Connect the water condensate removal hose provided (1 m (3.28 ft)) to the drain connection.

    NOTE: An external water condensate evaporator can be connected to the drain connection.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?