GEX8258701EN-01

Commissioning and Maintenance

DANGER
hazard of electric shock, explosion or arc flash
  • Disconnect all sources of power from the cooling unit before performing any maintenance.
  • Maintenance must be carried out by qualified personnel using original spare parts.
  • Use appropriate personal protective equipment (PPE) when performing maintenance.
  • Some tubes may be hot and can cause burns.
  • After performing maintenance, check that the ground wire of the cooling cover is still connected.
Failure to follow these instructions will result in death or serious injury.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?