GEX8258701EN-01

Transport and Storage

NOTICE
COMPRESSOR AND SEAL DAMAGE
During transport and storage:
  • Keep the cooling unit in the proper orientation indicated on the packaging during shipping and storage.
  • Do not expose the cooling unit to temperatures above 70 °C (158 ºF) or below -20 °C (-4 ºF), and/or relative humidity greater than 95%.
Failure to follow these instructions can result in equipment damage.

During transport and storage, the cooling unit must be kept in the position clearly stated on the kit:

  • vertically for side-mounted cooling units

  • horizontally for roof-mounted cooling units

Reception

Upon receipt, check that the packaging does not have shipping damage (for example, deterioration, cracks, scratches, or oil marks).

If there is any shipping damage, make a note of it on the acceptance receipt and notify the carrier.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?