DOCA0219EN-00

Testing the MicroLogic P Trip Unit

Test the trip unit using EcoStruxure Power Commission software installed on a PC and connected to the MicroLogic trip unit through the Service Interface.

Testing Architecture

  1. AC/DC power supply

  2. 7-pin cable for ComPacT NS trip units

  3. USB cable with magnet

For more information, refer to GDE78167 Service Interface - Instruction Sheet.

Test Functions with EcoStruxure Power Commission Software

EcoStruxure Power Commission software allows you to perform the following actions on a communicating MicroLogic trip unit through the Service Interface:

  • Automatic trip curve tests

  • Device check up (Force trip test)

  • Zone-selective interlocking (ZSI) test

  • Preparation for primary injection tests

For more information, refer to DOCA0170EN Service Interface - User Guide.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?