Alarms
-
An alarm may be viewed using:
-
The Alarm history menu.
-
The COM communications option.
-
-
The commands in the Protection menu are used to attribute a specific operating mode to each of the protection functions:
-
OFF: protection disabled
-
Alarm: the function issues an alarm, but does not trip the circuit breaker.
-
Trip + Alarm: the function issues an alarm and trips the circuit breaker.
-
-
The protection functions against overloads (long time), short circuits (short time and instantaneous) and ground faults (ground-fault and earth-leakage currents) automatically result in tripping and cannot be deactivated (Trip mode only).
-
The I
Alarm and phase rotation alarms can be set exclusively to OFF or Alarm mode.
-
The other protection functions for current, voltage, power and frequency may be set to any of the three modes, OFF, Alarm or Trip + Alarm.
-
The load shedding and reconnection function may be set to ON or OFF.
-
The resettable alarms linked to device tripping are activated when the Ir, Isd/Ii or I
thresholds are overrun.
-
The Ir alarm is reset one second after tripping. The Isd/Ii and
alarms are reset by pressing the
button.
-
Delayed alarms are activated when the pickup and dropout thresholds are overrun and the corresponding time delays have expired.
-
History logging
-
Alarm mode: as soon as a given protection threshold is overrun, an alarm is recorded in the Alarm history
-
Trip mode: as soon as a given protection threshold is overrun, the circuit breaker trips and the fault is recorded in the Trip history.
-
-
The Protection setup menu under History, maintenance and setup is used to enable or disable the Trip mode that is displayed in the protection-setting screens. On leaving the factory, the protection functions are set to Alarm mode.