DOCA0219EN-00

Voltage Protection Functions

The following voltage protection functions are available with the MicroLogic P trip unit.

  • Minimum voltage

  • Maximum voltage

  • Voltage unbalance

The voltage protection functions are set using the keypad. The settings are listed in Threshold and Time-Delay Settings.

Operating Principle

Protection tripped by a minimum value

Protection tripped by a maximum value

  1. Pickup threshold

  2. Pickup time delay

  3. Dropout threshold

  4. Dropout time delay

  • For protection tripped by a minimum or maximum value, it is possible to set:

    • A pickup threshold (1) that activates an alarm, a contact and/or tripping.

    • A pickup time delay (2) that steps in when the pickup threshold (1) is reached.

    • A dropout threshold (3) corresponding to deactivation of the alarm and/or contact.

    • A dropout time delay (4) that steps in when the dropout threshold (3) is reached.

  • For protection tripped by a minimum value, the dropout threshold is always greater than or equal to the pickup threshold.

  • For protection tripped by a maximum value, the dropout threshold is always less than or equal to the pickup threshold.

  • If both the minimum and maximum protection functions are activated at the same time, the minimum threshold is automatically limited to the value of the maximum and vice versa.

Minimum-Voltage Protection U min

  • This function calculates the minimum rms value of the three phase-to-phase voltages.

  • Protection is activated when at least one of the three phase-to-phase voltages (U12, U23, U31) is below the threshold set by the user.

  • This protection function does not detect phase failure.

NOTE: If the voltage protection functions are activated and the voltage measurement inputs are still energized, it is impossible to reset and close the circuit breaker.

Maximum-Voltage Protection U max

  • This function calculates the maximum rms value of the three phase-to-phase voltages.

  • Protection is activated when the three phase-to-phase voltages (U12, U23, U31) are simultaneously above the threshold set by the user.

Voltage-Unbalance Protection U unbal

This protection is activated by an adjustable level of unbalance between the rms values of the three phase-to-phase voltages.

This function calculates the rms value of the unbalance between the three phase-to-phase voltages.

U unbal = |E max|/U avg

Where:

  • U avg is the average value of the rms voltages of the three phases.

    U avg = (U12 + U23 + U31)/3

  • E max is the maximum difference between the voltage of each phase and U avg.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?