DOCA0219EN-00

Setting Load Shedding And Reconnection Function

The load shedding and reconnection function is set only using the keypad.

  1. Select > Load shedding I or > Load shedding P.

  2. Use the buttons below the display screen to enable or disable the function:

    • Off: load shedding is disabled

    • On: load shedding is enabled

  3. Use the buttons below the display screen:

    • To set the pickup threshold and time delay

    • To set the dropout threshold and time delay

For more information about the load shedding and reconnection function, see load shedding and reconnection.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?