Long-Time Rating Plug
One of the four interchangeable long-time rating plugs can be used to limit the long-time pickup setting range for higher accuracy of the long-time overcurrent protection.
Selecting the Long-Time Rating Plug
The available rating plugs are listed in the following table:
|
Part number |
Setting range for the Ir value |
|
|---|---|---|
|
C33542 |
Standard |
0.4 to 1 x Ir |
|
C33543 |
Low setting |
0.4 to 0.8 x Ir |
|
C33544 |
High setting |
0.8 to 1 x Ir |
|
C33545 |
Without long-time protection Ir = In for short-time protection setting |
|
-
The long-time current setting Ir is 0.4.
-
The long-time time delay tr corresponds to the value indicated by the adjustment dial.
-
The earth-leakage protection function is disabled.
-
The voltage-measurement inputs are disconnected.
Replacement Procedure
DANGER |
|---|
|
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Failure to follow these instructions will result in death or serious injury.
|
| NOTICE |
|---|
|
hazard of trip unit deterioration
Prior to running dielectric strength tests, it is mandatory
to:
Failure to follow these instructions can result in equipment damage.
|
Follow this procedure to change or remove the rating plug:
-
Open the circuit breaker.
-
Open the protective cover of the trip unit.
-
Record switch settings.
-
Unscrew the long-time rating plug mounting screw.
-
Remove the adjustable rating plug.
-
Inspect mounting area for debris and contamination.
-
Take out the replacement rating plug.
-
Gently push in the replacement rating plug.
-
Set trip unit settings to values recorded previously or modify settings.
DANGER