Tree Navigation
Tree Structure Screen Display
The navigation trees provide access to all the screens of MicroLogic P trip units.
The different screens are organized in branches corresponding to a given type of information.
The following branches are available, in the indicated order, depending on the type of MicroLogic trip unit:
Default Screen
All menu selections start at the default screen.
The default screen displays:
-
A bar graph representing the instantaneous values of the phase currents I1, I2, I3 and the neutral current IN (for 4–pole circuit breakers).
-
The value in amperes of the most heavily loaded phase. The number for that phase is presented in a square.
Navigating with the Keypad Buttons
Use the keypad buttons on the face of the MicroLogic P trip unit to navigate in the menu structure, and to access displayed values and configurable settings.
The possible operations are listed below:
-
Display data, for example, energy values
-
Reset values or counters, for example, reset the maximum power
-
Select options in a list, for example, language
-
Set protection functions, for example, long-time protection
Whatever the screen displayed, if no further action is taken, the system returns to the default screen after a few minutes.
Saving Settings
When a setting is changed in any of the three menus, pressing
one of the three buttons ,
or
displays the screen used to save the modification(s).
-
Select yes to save the modifications.
-
Select no to cancel and maintain the previous settings.
-
This screen is displayed until yes or no is selected.
Reset Maximum Values
The maximum values can be reset when they are displayed on the screen:
-
Press - to reset all maximum values displayed on the screen
-
Press + to cancel the reset and restore the maximum values