DOCA0219EN-00

MicroLogic P HMI Description

The human machine interface (HMI) of the MicroLogic P trip unit includes:

  • A graphic display screen

  • Buttons to navigate through the menu structure, and access monitored parameters and configuration settings

Display Screen and Buttons

The MicroLogic P trip unit includes the following display screen and buttons:

  1. Fault-trip reset and battery test button

  2. Digital display

  3. Metering menu button with LED

  4. History, maintenance and setup menu button with LED

  5. Scroll down or reduce displayed value button

  6. Scroll up or increase displayed value button

  7. Protection menu button with LED

  8. Menu selection button

Menu LEDs

The activated LED indicates the menu for which the screen is displayed:

  • Metering

  • History, maintenance and setup

  • Protection

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?