Neutral Protection
Three-Pole Circuit Breakers
Protection of the neutral is possible on a three-pole circuit breaker by connecting an external sensor.
For more information about the setting procedure, refer to Setting Neutral Protection.
|
MicroLogic trip unit |
5.0 P, 6.0 P and 7.0 P |
|||
|
Setting |
OFF (factory setting) |
N/2 |
N |
1.6xN |
|
Protection setting |
Description |
|---|---|
|
OFF: Neutral unprotected |
The distribution system does not require protection of the neutral conductor. |
|
N/2: Half neutral protection |
The cross-sectional area of the neutral conductor is half that of the phase conductors.
|
|
N: Full neutral protection |
The cross-sectional area of the neutral conductor is equal to that of the phase conductors.
|
|
1.6xN: Oversized neutral protection |
In installations with a high level of third-order harmonic currents (or multiples thereof), the current in the neutral conductor may exceed that of the phase currents under steady-state conditions
|
Four-Pole Circuit Breakers
For more information about the setting procedure, refer to Setting Neutral Protection.
|
MicroLogic trip unit |
5.0 P, 6.0 P and 7.0 P |
|||
|
Setting |
OFF |
N/2 (factory setting) |
N |
|
|
Protection setting |
Description |
|---|---|
|
OFF: Neutral unprotected |
The distribution system does not require protection of the neutral conductor. |
|
N/2: Half neutral protection |
The cross-sectional area of the neutral conductor is half that of the phase conductors.
|
|
N: Full neutral protection |
The cross-sectional area of the neutral conductor is equal to that of the phase conductors.
|