Load Shedding and Reconnection
The load shedding and reconnection function is set using the keypad, see Setting Load Shedding and Reconnection Function. The settings are listed in Threshold and Time-Delay Settings.
Load Shedding and Reconnection Depending on Current
The pickup curve for load shedding and reconnection depending on current is parallel to the I2t and Idmtl long-time curves. If a rating plug without long-time protection is installed, the load shedding and reconnection function based on current cannot be activated.
-
I2t long-time protection: the neutral is taken into account.
-
Idmtl long-time protection: the neutral is not taken into account.
The function does not trip the circuit breaker. It can be used to disconnect and reconnect non-priority loads by triggering an alarm linked to:
-
Outputs of the IO module
-
The communication option
The load-shedding and reconnection function is determined by thresholds and time delays.
The pickup threshold is always greater than or equal to the dropout threshold.
Load Shedding and Reconnection Depending on Power
Load shedding and reconnection depending on power calculates the total active power on the three phases. The function does not trip the circuit breaker. It can be used to disconnect and reconnect non-priority loads by triggering an alarm linked to:
-
Outputs of the IO module
-
The communication option
The load-shedding and reconnection function is determined by thresholds and time delays.
The pickup threshold is always greater than or equal to the dropout threshold.