DOCA0219EN-00

Power, Energy, and Frequency

Instantaneous Power and Power Factor

The MicroLogic P trip unit offers a number of different measurements.

  • Total power measurements:

    • Instantaneous active power P in kW

    • Instantaneous reactive power Q in kvar

    • Instantaneous apparent power S in kVA

  • Measurement of the power factor PF

To ensure reliable power and power-factor measurements, the Power sign and Sign convention parameters must be set.

NOTE: For the measurement ranges and accuracies, see Measurement Ranges and Accuracy .

Demand Power

  • Display of the demand values for the active power P, reactive power Q and apparent power S

  • Selection of the demand calculation method

  • Display of the interval over which the value is calculated

  • The maximum demand values are displayed and stored in memory.

  • The stored maximums can be reset at any time.

NOTE:
  • The calculation method, the type of calculation window (fixed or sliding) and its duration may be set in the Metering setup menu under History, maintenance and setup.

  • The synchronisation function (Synchro.Com) is available only with the COM communication option. With this function, the demand power is determined on the basis of a signal synchronized by the communication module.

  • These settings apply to all demand powers (active power P, reactive power Q and apparent power S). If the settings are modified, the demand values are systematically recalculated.

Energy

The MicroLogic P trip unit offers a number of different measurements.

  • Total energy:

    • Total active energy E.P in kWh

    • Total reactive energy E.Q in kvarh

    • Total apparent energy E.S in kVAh

  • Energy consumed (Energy in), positively incremented:

    • Active energy E.P in kWh

    • Reactive energy E.Q in kvarh

  • Energy supplied (Energy out), negatively incremented:

    • Active energy E.P in kWh

    • Reactive energy E.Q in kvarh

  • Energy values can be reset.

NOTE:
  • The Energy in and Energy out values are incremented according to the power sign set in the Metering setup menu under History, maintenance and setup.

  • As standard, the total calculated energy values are absolute total values. They represent the sum of the energy in and out values:

    • E.P = Σ E.P in + Σ E.P out

    • E.Q = Σ E.Q in + Σ E.Q out

  • As an option (access exclusively via the COM communications option), energy can be calculated algebraically:

    • E.P = Σ E.P in - Σ E.P out

    • E.Q = Σ E.Q in - Σ E.Q out

    These values are called signed energies.

Frequency

The frequency of the distribution system is displayed in Hz.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?