Earth-Leakage Protection on MicroLogic 7.0 P Trip Unit
-
The earth-leakage protection function primarily helps to protect people against indirect contact because an earth-leakage current can provoke an increase in the potential of the exposed conductive parts.
-
The earth-leakage pick-up value IΔn is displayed directly in amperes and the time delay follows a constant-time curve.
-
An external rectangular sensor is required for this function.
-
This function is inoperative if the long-time rating plug is not installed.
-
As a type-AC, the circuit breaker is protected against nuisance tripping.
-
As a type-A, the circuit breaker provides DC-component withstand up to 10 A.
-
If the optional external voltage-measurement input is used, a 24 Vdc external power supply must be connected to the F1-/ F2+ terminals, see Power Supply
. -
For the factory settings, the setting ranges, increment steps and setting accuracies, see Threshold and Time-Delay Settings.
Pick-Up Value IΔn
|
IΔn pickup (A) (accuracy 0 to - 20%) |
0.5 |
1 |
2 |
3 |
5 |
7 |
10 |
20 |
30 |
Time Delay Δt
|
Δt time delay (ms) (Maximum resettable time) |
60 |
140 |
230 |
350 |
800 |
|
Δt Maximum break time (ms) |
140 |
200 |
320 |
500 |
1000 |