Setting Up the MicroLogic Trip Unit
Prior to setting up the protection functions or carrying out measurements, set up the following parameters of the MicroLogic trip unit:
-
Display language
-
Date and time
-
Circuit breaker type
-
Power sign
-
Transformation ratio between the primary and secondary windings (if an auxiliary voltage transformer is installed)
-
Rated frequency
Selecting the Display Language
Returning to English
-
Return to the default screen by pressing any of the three buttons without a lit LED:
-
Select the History, maintenance and setup menu by pressing
.
-
Move the cursor to the first menu item and then down to the third menu item to select the MicroLogic setup menu .
-
Select Language by moving the cursor up to the first menu item. Press
to confirm the selection.
-
Select English from the list and confirm the selection.
Setting the Date and Time
Follow this procedure to set the date and time of the MicroLogic trip unit. The date and time are used for time-stamping in the trip and alarm histories.
If time is not synchronized via the communication module, a drift of up to one hour per year may be observed.
Selecting the Circuit Breaker
Follow this procedure to set the characteristics of the circuit breaker.
Selecting the Sign of the Power
By default, the MicroLogic P trip unit uses P+ for the power flowing from top to bottom terminals. The selected direction of flow is valid for:
-
Measurement of power and the power factor
-
Measurement of energy
-
Load shedding and reconnection depending on power
Entering the Voltage-Transformation Ratio
If the supply voltage for the trip unit exceeds 690 V, install a PTE external voltage measurement input option and an external voltage transformer.
If an external voltage transformer is installed, to display the true voltage values, enter the transformation ratio between the primary and secondary voltages of the transformer.
Entering the Rated Frequency
|
Step |
Action |
|
|---|---|---|
|
1 |
||
|
2 |
||
|
3 |
||
|
4 |
Use the navigation buttons to access and set the frequency. |
|