LEDs and Display Screens
MicroLogic P trip units are equipped with overload and fault indication LEDs.
Overload LED
The overload LED indicates that the long-time current setting Ir has been overrun. The bar graph displays the overload as a percentage of Ir. The load level on each phase is displayed, with the most heavily loaded phase outlined.
-
Overload bar graph on the default screen
-
LED Indicator
Trip Cause Indications
A trip is signalled by the following means:
-
Trip cause indication LEDs
-
Trip cause notification displayed on the screen
The trip cause notifications depend on the following factors:
-
The presence of an external power supply. For more information about external power supplies, refer to Power supply.
-
The connection of voltage measurement inputs upstream or downstream.
Trip Cause Indication LEDs
The indications of the four trip cause LEDs depend on the type of MicroLogic trip unit.
When activated, a LED remains ON until it is locally reset.
-
A number of simultaneous causes may result in tripping. The LED signalling the last trip cause chronologically is the only one to remain ON.
-
The battery maintains the trip cause indications. If there are no indications, check the battery.
Resetting Trip Cause Indications
-
Determine why the circuit breaker tripped. The trip cause indication is maintained until it is reset on the trip unit.
For more information about the procedure for resetting and closing the circuit breaker after a trip, refer to DOCA0221EN ComPacT NS - Circuit Breakers and Switch-Disconnectors - User Guide.