DOCA0219EN-00

Viewing the Operation Counter and Contact Wear Indicator

Viewing and/or Resetting the Operation Counter

Select the command Event history > Operation counter

Reset...

then

... or cancel the reset, then confirm.

Checking the Contact Wear

Select the command Event history > Contact wear

NOTE: Contact wear is indicated from 0 to 900. The contacts should be inspected every time the counter reaches a multiple of 100.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?