Setting Principles
With the protective cover open, make all the necessary settings for your trip unit:
-
Use the dials to set MicroLogic P protection thresholds and time delays for overloads, short-circuits, ground faults and earth leakage.
If the set thresholds are overrun, these protection functions systematically trip the circuit breaker.
-
Use the buttons on the keypad:
-
For fine adjustments of the protection thresholds and time delays for overloads, short-circuits, ground faults and earth leakage. The value previously set using a dial automatically becomes the maximum value for the keypad settings
-
To activate and set the MicroLogic P functions not accessible via the dials.
-
With the protective cover closed, it is not possible to set the protection functions. However, it is possible to set metering functions and alarms, as well as view all measurements, settings and histories.
For remote settings using the communication option, see the Remote settings section in the Com setup menu under History, maintenance and setup.
Setting Protection Functions Using the Dials
-
Deletes all the fine adjustments previously made using the keypad for the overload (long-time) and short-circuit (short-time and instantaneous) protection.
-
Does not affect the fine adjustments made using the keypad for ground-fault and earth-leakage protection.
-
Does not affect any other settings made using the keypad.
Similarly, a new ground-fault or earth-leakage protection setting made using one of the dials:
-
Deletes all the fine adjustments previously made using the keypad for the ground-fault and earth-leakage protection.
-
Does not affect the fine adjustments made using the keypad for the overload (long-time) and short-circuit (short-time and instantaneous) protection.
-
Does not affect any other settings made using the keypad.
Setting Protection Functions Using the Keypad
Locking Access to Protection Settings
The protection settings are locked when the protective cover is closed to prevent access to the adjustment dials and to disable fine adjustments using the keypad.
If necessary, install a lead seal to protect the settings.
With the protective cover closed, it is possible to set metering
functions and alarms, as well as view all measurements, settings and
histories using the keypad.