Metering Menu
Description
The Metering menu contains the following submenus:
| Level 1 | Level 2 | Function description |
|---|---|---|
| Default screen |
I (A) |
Current measurements |
|
U (V) |
Voltage measurements | |
|
P (kW) |
Power measurements | |
|
E (kWh) |
Energy measurements | |
|
F (Hz) |
Frequency measurements |
Navigation
Use the buttons below the display screen to navigate the menus.
Current Measurements
|
Level 2 |
Level 3 |
Level 4 |
Description |
|---|---|---|---|
|
I (A) |
I inst |
I1 I2 I3 IN |
(depending on the type of system) |
| Max |
Storing and reset of the maximum instantaneous currents |
||
|
Demand |
I1 I2 I3 IN |
(depending on the type of system) |
|
| Max |
Storing and reset of the maximum demand currents |
Voltage Measurements
|
Level 2 |
Level 3 |
Description |
|---|---|---|
|
U (V) |
Instant. |
Instantaneous phase-to-phase U12, U23, U31 and phase-to-neutral V1N, V2N, V3N voltages (depending on the type of system) |
|
Average 3 Φ |
Average voltage U average of the phase-to-phase voltages. |
|
|
Unbal 3 Φ |
Unbalance voltage U unbal. of the phase-to-phase voltages. |
|
|
Phase rotation |
Phase sequence |
Power Measurements
|
Level 2 |
Level 3 |
Level 4 |
Description |
|---|---|---|---|
|
P (kW) |
P inst. |
P, Q, S |
|
|
Power factor |
Power factor PF |
||
|
Demand |
P, Q, S |
Demand values for:
|
|
| Max |
Storing and reset of the maximum demand power values |
Energy Measurements
|
Level 2 |
Level 3 |
Description |
|---|---|---|
| E (kWh) |
E total |
|
|
E in |
Positive component of:
|
|
|
E out |
Negative component of:
|
|
|
Reset Energy |
Reset all the energy values to zero. |
Frequency Measurements
|
Level 2 |
Description |
|---|---|
|
F (Hz) |
Frequency F |