Checking and Replacing the Battery
Checking the Internal Battery
Press and hold down the test button on the trip unit to check the LEDs and the battery. The battery information is displayed if the trip unit is equipped with an external power supply or if the circuit breaker is ON.
Internal Battery
If the MicroLogic P battery needs to be changed, order a new battery in its housing cover with the Schneider Electric catalogue number 33593.
-
Lithium battery
-
1/2 AA, 3.6 V, 900 mA/h
-
Ambient temperature: -55 °C to 130 °C (-67 °F to 266 °F)
Replacing the Internal Battery
DANGER |
|---|
|
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Failure to follow these instructions will result in death or serious injury.
|
Follow this procedure to replace the internal battery:
-
Remove the circuit breaker front cover as directed in the circuit breaker instruction sheet.
-
Remove the battery and its housing cover: insert a small screwdriver blade into battery housing cover notch and rotate to slide battery housing cover out of trip unit.
-
Reinstall the circuit breaker front cover as directed in the circuit breaker instruction sheet.
DANGERHAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH- Put back circuit breaker front cover before energizing circuit breaker to help prevent access to live terminals.
- Do not pinch the wires when reinstalling the front cover.
Failure to follow these instructions will result in death or serious injury.