DOCA0219EN-00

Description

  1. Top fastener

  2. Terminal block for external connections

  3. Battery compartment

  4. Lead-seal fixture for protective cover

  5. Protective cover

  6. Bottom fastener

  7. QR code on protective cover, to access product information

  8. Cover opening point

  9. Screw for long-time rating plug

  10. Long-time rating plug

  11. Infrared link with communication interface

  12. Connection with circuit breaker

 

MicroLogic 5.0 P Trip Unit

  1. Long-time trip cause indication LED

  2. Short-time or instantaneous trip cause indication LED

  3. Additional protection or auto-protection trip cause indication LED

  4. Fault-trip reset and battery test button

  5. Digital display

  6. Metering menu button with LED

  7. History, maintenance and setup menu button with LED

  8. Scroll down or reduce displayed value button

  9. Scroll up or increase displayed value button

  10. Protection menu button with LED

  11. Menu selection button

  12. LED indicating an overload

  13. Long-time current setting lr

  14. Long-time time delay tr

  15. Short-time pickup lsd

  16. Short-time time delay tsd

  17. Instantaneous pickup li

  18. Test connector

MicroLogic 6.0 P Trip Unit

  1. Long-time trip cause indication LED

  2. Short-time or instantaneous trip cause indication LED

  3. Ground-fault trip cause indication LED

  4. Additional-protection or auto-protection trip cause indication LED

  5. Fault-trip reset and battery test button

  6. Digital display

  7. Metering menu button with LED

  8. History, maintenance and setup menu button with LED

  9. Scroll down or reduce displayed value button

  10. Scroll up or increase displayed value button

  11. Protection menu button with LED

  12. Menu selection button

  13. LED indicating an overload

  14. Long-time current setting lr

  15. Long-time time delay tr

  16. Short-time pickup lsd

  17. Short-time time delay tsd

  18. Ground-fault pickup lg

  19. Ground-fault time delay tg

  20. Instantaneous pickup li

  21. Test button for ground-fault protection

  22. Test connector

MicroLogic 7.0 P Trip Unit

  1. Long-time trip cause indication LED

  2. Short-time or instantaneous trip cause indication LED

  3. Earth-leakage trip cause indication LED

  4. Additional-protection or auto-protection trip cause indication LED

  5. Fault-trip reset and battery test button

  6. Digital display

  7. Metering menu button with LED

  8. History, maintenance and setup menu button with LED

  9. Scroll down or reduce displayed value button

  10. Scroll up or increase displayed value button

  11. Protection menu button with LED

  12. Menu selection button

  13. LED indicating an overload

  14. Long-time current setting lr

  15. Long-time time delay tr

  16. Short-time pickup lsd

  17. Short-time time delay tsd

  18. Earth-leakage pickup IΔn

  19. Earth-leakage time delay Δt

  20. Instantaneous pickup li

  21. Test button for earth-leakage protection

  22. Test connector

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?