DOCA0219EN-00

Event Histories

Trip History

  • The trip history is the means to display at any time the parameters measured during the last ten trips.

  • For each trip, the following parameters are recorded:

    • Tripping cause

    • Trip threshold

    • Interrupted currents in amperes (only if an external power supply is present) for Ir, Isd/Ii, Ig or IΔn trips

    • Date

    • Time (hours, minutes and seconds)

NOTE: The interrupted currents are indicated in terms of their peak values.

Alarm History

  • The alarm history is the means to display at any time the parameters measured during the last ten alarms.

  • For each alarm, the following parameters are recorded:

    • Alarm cause

    • Alarm threshold

    • Date

    • Time (hours, minutes and seconds)

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?