Setting MicroLogic 7.0 P Trip Unit
You can set the tripping curve of your MicroLogic 7.0 A trip unit to match the needs of your installation using the following parameters:
-
Long-time current setting Ir
-
Long-time time delay tr
-
Short-time pickup Isd
-
Short-time time delay tsd
-
Instantaneous pickup Ii
-
Earth-leakage pickup IΔn
-
Earth-leakage time delay Δt
Set the Threshold Values Using the Dials
In this example, the rated current In of the circuit breaker is 2000 A.
Set the Time Delays Using the Dials
In this example, time delay tr of the circuit breaker is 1 second, time delay tsd is 0.2 seconds with I²t short-time ON and time delay Δt = 140 milliseconds
Adjusting Protection Settings Using the Keypad
To adjust the settings of the long-time, short-time, and instantaneous protection functions, refer to MicroLogic 5.0 P settings.
To adjust the settings of the earth-leakage protection function:
-
Use the buttons below the display screen to select, confirm, and save the settings.