DOCA0219EN-00

Testing the Ground-Fault and Earth-Leakage Functions

Proceed as follows to test:

  • Ground-fault protection on MicroLogic 6.0 P trip unit

  • Earth-leakage protection on MicroLogic 7.0 P trip unit

  1. Check that the circuit breaker is closed.

  2. Use a thin screwdriver to briefly push in (< 1 s) the TEST button on the front face of the MicroLogic trip unit.

  3. The circuit breaker trips.

  4. If the circuit breaker does not trip, contact your field service representative.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?