Setting Up the Metering Functions
Prior to setting up the protection functions or carrying out measurements, set up the following parameters of the MicroLogic trip unit:
-
System type
-
Calculation mode for the demand current
-
Calculation mode for the demand power
-
Power factor sign convention
Selecting the System Type
The MicroLogic P trip unit offers three measurement options, as indicated in the table. The availability of measurements depends on the option selected.
|
Measurement type |
Currents on phases I1, I2, I3 |
Current on neutral IN |
Phase-to-phase voltages U12, U23, U31 |
Phase-to-neutral voltages V1N, V2N, V3N |
|---|---|---|---|---|
|
3 phases, 3 wires, 3 CTs (method using two wattmeters) |
✔ |
– |
✔ |
– |
|
3 phases, 4 wires, 3 CTs (method using three wattmeters) |
✔ |
– |
✔ |
✔ |
|
3 phases, 4 wires, 4 CTs (method using three wattmeters) |
✔ |
✔ |
✔ |
✔ |
|
Step |
Action |
|
|---|---|---|
|
1 |
||
|
2 |
||
|
3 |
Use the navigation buttons to access and set the System type. |
|
For a 3-pole device, the neutral, if distributed, must be connected to terminal VN of the MicroLogic P trip unit.
For more information about types of measurements, refer to Measurements.
Selecting the Calculation Method for Demand Current
Selecting the Calculation Method for Demand Power
Setting Up the Power-Factor Calculation
|
Step |
Action |
|
|---|---|---|
|
1 |
||
|
2 |
||
|
3 |
Use the navigation buttons to access and set the Sign convention.
|
|