Setting Up the COM Communications Option
| NOTICE |
|---|
|
hazard of loss of communication
Do not change the communication parameters on a system
in operation.
Failure to follow these instructions can result in data
loss.
|
The communication parameters have default values that can or must be changed according to the needs of the installation or users.
When a COM communications option is used, it is necessary to:
-
Set up the COM communications option.
-
Authorize remote setting of the MicroLogic trip unit.
-
Authorize remote control of the circuit breaker.
Setting Up the Modbus Address
The Modbus address is a two-digit number identifying the MicroLogic P trip unit in a Modbus network.
The setting of the Modbus address depends on the COM option.
|
COM option |
Modbus address |
Modbus address range |
|---|---|---|
|
BCM or BCM ULP not connected to IFM or IFE |
The Modbus address is set up on the Modbus Com setting screen, with the parameters of the communication option (see below). |
1 to 47 |
|
BCM ULP connected to IFM |
The Modbus address is set up on the 2 address rotary switches on the front panel of the IFM. |
1 to 99 Value 0 is forbidden because it is reserved for broadcasting messages. |
|
BCM ULP connected to IFM with legacy firmware |
The Modbus address is set up on the 2 address rotary switches on the front panel of the IFM. |
1 to 47 Value 0 is forbidden because it is reserved for broadcasting messages. Values 48 to 99 are not allowed. |
|
BCM ULP connected to IFE |
The Modbus address is fixed and cannot be changed. |
255 |
Authorizing Remote Setup of MicroLogic
To authorize the remote setup of the MicroLogic trip unit equipped with a BCM or BCM ULP, access permit must be set to YES on the Remote settings screen.
If the operator does not enter a specific access code, the default access code is 0000 and is requested by the supervisor.
Authorizing Remote Control of the Circuit Breaker
|
Step |
Action |
|
|---|---|---|
|
1 |
||
|
2 |
||
|
3 |
Use the navigation buttons to access and set Remote control.
|
|
|
4 |
||
To authorize the remote control of the circuit breaker, Auto must be set on the Remote control screen.
If the circuit breaker is connected to other ULP modules, each ULP module must be set to authorize the remote control of the circuit breaker:
-
On FDM121 display unit, set the circuit breaker in remote control mode on the FDM121 Control menu
-
On IO module with predefined application 2 (breaker application), set the selector switches connected to the IO module inputs to:
-
Remote control mode (I1 = 1)
-
Enable close order (I4 = 1)
-
-
On IFM or IFE communication interface, the IFM or IFE locking pad must be set on UNLOCK (padlock open).
For more information on the communication option, refer to the:
-
ULP system user guide.
-
IO module user guide.
-
IFE user guide.
-
FDM121 user guide.