DOCA0219EN-00

Power Supply

Internal and External Power Supplies

The MicroLogic trip unit is powered by the current through the internal current transformers (CT).

  • The standard protection functions of MicroLogic trip units operate with the internal current supply.

  • If the load current is higher than 20% of the rated current In, the internal current supply provides the power supply for the full functioning of the MicroLogic trip unit. This includes:

    • The MicroLogic HMI, display screen and LEDs

    • The metering functions

To provide a power supply to the MicroLogic trip unit when the load is below 20% of the rated current In, and maintain the full functioning of the MicroLogic trip unit, a permanent external 24 Vdc power supply can be used.

External 24 Vdc Power Supply

The 24 Vdc power supply maintains the operation of all functions of the MicroLogic trip unit in all circumstances, even when the circuit breaker is open and not energized.

The 24 Vdc power supply maintains the functions of the MicroLogic trip unit in low load conditions (load below 20%).

NOTICE
loss of double insulation
  • Supply the MicroLogic trip unit with a 24 Vdc SELV (Safety Extra Low Voltage) power supply only, connected to the F1-/F2+ terminals. Pay attention to the polarity.
  • Do not connect devices which have double insulation to the 24 Vdc SELV power supply which is being used to supply the MicroLogic trip unit. For example, do not use the same 24 Vdc SELV power supply to supply a MicroLogic trip unit for ComPacT NS circuit breakers and a MicroLogic X control unit for MasterPact MTZ circuit breakers.
Failure to follow these instructions will result in a basic/single insulated system.
NOTICE
hazard of equipment damage
  • Do not use the same 24 Vdc SELV power supply to supply the MicroLogic trip unit and the other ULP modules connected to the BCM ULP module.
  • Do not use the same 24 Vdc SELV power supply to supply more than one MicroLogic trip unit.
Failure to follow these instructions can result in equipment damage.

Recommendations for use of external 24 Vdc SELV power supplies:

  • Use separate 24 Vdc power supplies to supply each MicroLogic trip unit. You can use the same 24 Vdc power supply to supply the ULP modules in several Intelligent Modular Units (IMU).

  • Use a separate 24 Vdc power supply to supply the MN or MX voltage releases.

Recommended 24 Vdc Power Supply

The following 24 Vdc power supply is recommended for use with ComPacT NS devices. For more information, refer to the ComPacT NS Catalogue.

Characteristic

AD power supply

Illustration

Overvoltage category defined by IEC 60947-1

  • Category IV per IEC 62477-1 (Vac model)

  • Category III per IEC 62477-1 (Vdc model)

  • Category III per UL 61010-1

Input supply voltage AC

  • 110–130 Vac

  • 200–240 Vac

Input supply voltage DC

  • 24–30 Vdc

  • 48–60 Vdc

  • 100–125 Vdc

Dielectric withstand

Input/output:

  • 3 kV RMS for 1 minute (110–130 Vac and 200–240 Vac model)

  • 3 kV RMS for 1 minute (110–125 Vdc model)

  • 2 kV RMS for 1 minute (24–30 Vdc and 48–60 Vdc model)

Temperature

70 °C (158 °F)

Output current

1 A

Ripple

200 mV peak-peak

Output voltage setting for line loss compensation

22.8–25.2 Vdc

24 Vdc Backup Battery

If the 24 Vdc power supply is interrupted, a 24 Vdc backup battery can be used to maintain the operation of the MicroLogic trip unit. It is installed in series between the MicroLogic trip unit and the 24 Vdc power supply module.

The 24 Vdc backup battery must have the following characteristics (compatible with the MicroLogic trip unit):

  • Output voltage 17–28.8 Vdc

    • Cut-off voltage 17 Vdc (24 Vdc backup battery must have a shutdown output voltage in case of low voltage level)

    • Hysteresis > 3 Vdc (to avoid power-on before the voltage is up to 21 Vdc)

  • 24 Vdc backup battery should be able to power an Inrush current of 10 A

Internal Battery

When no other power supply is supplying the MicroLogic trip unit, the internal battery powers the trip cause LEDs.

ULP Module Consumption

The same power supply can be used to supply the ULP modules of several intelligent modular units (IMU).

The following table lists the ULP module consumption:

Module

Typical consumption (24 Vdc at 20 °C/68 °F)

Maximum consumption (19.2 Vdc at 60 °C/140 °F)

BCM ULP circuit breaker communication module for MasterPact NT/NW and ComPacT NS circuit breakers

40 mA

300 mA

IFE Ethernet interface for one circuit breaker

100 mA

140 mA

IFE Ethernet switchboard server

100 mA

140 mA

IFM Modbus-SL interface or one circuit breaker

21 mA

30 mA

FDM121 front display module for one circuit breaker

21 mA

30 mA

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.