Current and Voltage
Instantaneous Current
MicroLogic P trip units offer two, non-exclusive measurement possibilities.
-
On the bar graph displayed on the default screen
-
The instantaneous current of the most heavily loaded phase is automatically displayed in amperes for phases 1, 2, 3 and the neutral (depending on the neutral protection settings). The bar graph indicates the percent load of the three phases.
-
-
In the I inst. section of the instantaneous currents
-
Display in amperes of the instantaneous currents I (rms) on phases I1, I2 and I3 and the neutral current IN, the ground-fault current Ig (MicroLogic 6.0 P), the earth-leakage current IΔn (MicroLogic 7.0 P)
-
The maximum instantaneous currents are displayed and stored in memory.
-
The stored maximums can be reset at any time.
-
Demand Current
-
Display of the demand current on phases I1, I2, I3 and the neutral IN (depending on the type of distribution system)
-
Selection of the demand calculation method
-
Display of the interval over which the value is calculated
-
The maximum demand values are displayed and stored in memory
-
The stored maximums can be reset at any time.
Phase-to-Neutral and Phase-to-Phase Voltages
The MicroLogic P trip unit offers different voltage measurements:
-
Phase-to-phase voltages (rms) between phases U12, U23 and U31, displayed in volts
-
Phase-to-neutral voltages (rms) between the phases and the neutral V1N, V2N and V3N, displayed in volts.
For more information about voltage measurement inputs, refer to Selection of the Voltage-Measurement Inputs.
The supply circuit of the voltage-measurement input is reserved exclusively for the trip unit and must never be used to supply other circuits.
Average Voltage
Average U avg of the instantaneous voltages between phases U12, U23 and U31.
Phase Rotation
Display of the phase sequence.
Voltage Unbalance
Display of the unbalance U unbal between the three phase-to-phase voltages, displayed as a percentage.